Eaton Logo

Can the fuse clip and fuses be added to the EBMBB FD or EBMBD FD if they originally ordered without?

The mounting plate is already set up to accommodate the fused and non-fused versions of the DS switch within a given enclosure size. The fuse block and clips needs to be sourced from a Eaton/Cutler Hammer distributor IF they are available as a stand alone kit. The 100 amp verision came with the DS36U disconnect.  If the fuse block kit is not available, a complete DS363R would need to be ordered from Eaton which is the fused version.