Eaton Logo

Control

What are the replacement cover screws for DSD series covers.

Do you have intrinsically safe light switches?

Do you offer an explosion proof timer switch

Looking for an emergency stop button explosion-proof.

What is the replacement for our part EFSC218?

What is the minimum temperature rating for the EID Disconnect switches?

Where can I go to buy replacement parts or equivalent products to the old Crouse-Hinds Distribution Equipment Division (DED) products that were made in Earlysville, Virginia many years ago?

Does Crouse Hinds offer a single phase disconnect switch?

Do you have a cut sheet on DSD SID K1?

On the GFS1 can we get only the switch?

What are the components needed to order a factory sealed EDS2129?

What is the replacement for our part EFSC2129?

What is the replacement for the EFS1129?

What is the difference between parts DS415 and DS415A?

Does Crouse-Hinds offer a nameplate mounting bracket for control stations?

What is an ESWP126 K1?

On a 3 position selector switch, do you offer a spring return to center from both left and right?

What is the weight on a AFM211060?

What is the Crouse Hinds equivalent to Appleton ACSE Series part #: ACSE040805SQD13?

Dimensions needed for Crouse Hinds material#: GHG 411 8100 R0002.

Is the push button on an EFS1184 maintained?

Are your combination starters (EBM) factory wired between the breaker, starter and primary side of the control power transformer? If no, can it be done by way of special request?

I need an Emergency Stop pushbutton station for a hazardous location

I need a data sheet for a model GHG432 KLM00 SGT551206F/0033

What is the replacement knob used on DSD, EDS, EFD selector switches?

Can the SX178 lockout be added in the field to DSD SR control stations?

What is the replacement part number for the buzzer used on AFK211060?

are GHG273 series light switches available in 4-way?

Does the DS652 have hazardous area markings on the cover?

Is there a HP rating for the EDS2129?

What did the suffix S16 on an EFS/EFD control station represent?

Need the wiring diagram for the DSD TS timer.

Can custom markings be ordered for EDS Control Station Covers

Can the DSD TS timers be sold in the US?

Is there a replacement part number for the horn used in an AFK211060?

What temperature range is acceptable for EDS, EFD control stations?

Can our EMP operators be used with our NJB enclosures?

What type of stainless steel is used for the DSD SCREWPACK?

I am looking for a Control Station that can withstand -40 F weather.

I have a DS443 SA and a DEV42 two position switch to build a Flexstation control station, however, the selector switch does not appear to be long enough to operate the contacts. Why?

Do the EMPS/EMP key operated barrel switches share the same physical key type? If I bought three of these, will one key be able to work with all three?

What is the UL certification number for an EFD/EFDC hazardous area circuit breakers?

Are the Eaton Crouse - Hinds EFD/EFDC series breaker enclosures UL listed?

Is there a datasheet for Part # DS SST NPBRKT:1292448?

What is the DC rating of an SW5 factory sealed snap switch?

Can ESWP126's be stacked?

Does Crouse-Hinds offer a replacement for part number DSFS934 SA?

What is the material that closure plug part number DS:0206765 is made of?

What is the replacement part for the cover bolts on the EBM?

Has the ED1NP been replaced by another adder?

What is the fuse type and size for the transformer (CPT size 0-2) for our EBM Combo breaker/starter?

Does Crouse HInds offer a cross for Killark part number FXS-52D?

Does Eaton Crouse - Hinds offer a replacement for the ESH 4?

What is the switch that is used in a GUSC2013?

Is there a lockout provision for Crouse Hinds EMP's?

Does Crouse-Hinds have a replacement spring for the DSD TS 11M60SA?

What is the amp rating for an EDSC21102 motor starter?

Crouse-Hinds part number, DSP1 , is no longer offered. Does Crouse-Hinds recommend a replacement?

What kind of switch does the DSD-TS Series Timers use?

Do you have installation instructions for the CHW53197A, CHW53198A and CHW53198 slack condition belt alignment switches?

Do you have installation instructions for the CHW53198B conveyor ripped belt switch?

Do you have installation instructions for the CHW93053 and CHW93058 IEC belt alignment switch?

Do you have installation instructions for the CHW53197 and CHW53197 IEC conveyor switch?

Is Pushbutton #DEV11 a momentary contact type?

Is the EDS2129 now rated for group B without the GB suffix?

Can you please confirm what ampacity the #DSD924 selector switch is rated for?

Does the EDSC21100 0 break down into components? If so what are the components?

What is the replacement for a EMP10 J1?

What did the suffix S768 represent?

What did the suffix S349 represent?

What is the replacement lens for the EMPX-009 J11 pilot light?

What is the replacement lens for the EMPX-009 J6 pilot light?

What is the replacement lens for the EMPX-009 J3 pilot light?

What is the replacement lens for the EMPX-009 J1 pilot light?

Can the lens on an EMPXS operator be be replaced?

Does Crouse-Hinds offer a cross for Killark Part # EXH1A10?

What is the part number for the replacement handle assembly for NCB1426F WT400LB 36?

Will a EMP009 work with a DS441 ?

Does Crouse Hinds offer a yellow maintained mushroom head?

What is the maximum conductor size for SW5 sealing well?

Do we offer DC voltage for the DSD TS timer?

Do you have the installation instructions for the CHW53198 conveyor belt trip switch?

Do you have the installation instructions for the CHW53197 conveyor belt trip switch?

Is there a replacement for the discontinued rocker handle control station MC2810?

Is there a replacement for the discontinued rocker handle control station MCC1810?

Is there a replacement for the discontinued rocker handle control station MC1810?

Is there a replacement for the discontinued rocker handle control station MCC2810U?

Is there a replacement for the discontinued rocker handle control station MCC1810U?

Is there a replacement for the discontinued rocker handle control station MC2810U?

Is there a replacement for the discontinued rocker handle control station MC1810U?

Is there a replacement for the discontinued rocker handle control station MCC2810U1?

Is there a replacement for the discontinued rocker handle control station MCC1810U1?

Is there a replacement for the discontinued rocker handle control station MC2810U1?

Is there a replacement for the discontinued rocker handle control station MC1810U1?

What are the replacement mounting feet for the EGL210 J1 J3 shown in the spec sheet attached.

Does the ACE-DG1-5 VFD require the fan/blower?

If you order EDS2190 S153, will both buttons come with a lockout?

Does the DS429 come with a contact block?

What is the recommended replacement for the EPC387 series circuit breaker enclosure?

What is the recommended replacement for the EPC377 series circuit breaker enclosure?