Eaton Logo

What is the lowest ambient temperature that you can apply Chico speed seal

CHICO SpeedSeal compound must be between 50°F (10°C) and 85°F (29°C) before mixing. Sealing fittings must be at a temperature above 40°F (4°C).